IEEE 802.16 OFDM Demod Properties Dialog Box

The 802.16 OFDM Demod Properties dialog box contains parameters that configure the VSA to demodulate 802.16 OFDM Orthogonal Frequency Division Multiplexing: OFDM employs multiple overlapping radio frequency carriers, each operating at a carefully chosen frequency that is Orthogonal to the others, to produce a transmission scheme that supports higher bit rates due to parallel channel operation. OFDM is an alternative tranmission scheme to DSSS and FHSS. modulated signals.

The 802.16 OFDM demodulator must be selected before this dialog box is available. To enable the demodulator, click Analysis > Type > Wireless Connectivity > IEEE 802.16 OFDM.

The IEEE 802.16 OFDM Demod Properties dialog box contains these tabs:

See Also

Selecting the 802.16 OFDM Demodulator

Setting up an 802.16 OFDM measurement