Format Tab (802.16 OFDM)
The tab of the dialog box configures the VSA's demodulator. These are the parameters necessary for the VSA to lock on to and demodulate the test signal.
The tab dialog box configures these parameters:
- Data Subcarrier Modulation Format
- Guard Interval
- Manual Fs/BW Ratio
- Nominal Bandwidth
- Preset to Standard
- Standard
See Also
IEEE 802.16 OFDM Demod Properties