Eq Impulse Response (802.16 OFDM)

Eq Impulse Response shows the impulse response of the equalization filter. How the Eq Impulse Response is computed depends on the selection for the Equalizer Training parameter Analysis > IEEE 802.16 OFDM Demod Properties > Advanced tab. If the Equalizer Training parameter is set to Preamble Only, the Eq Impulse is computed using just the Channel Estimation Sequence portion of the preamble. If the parameter is set to Preamble & Data, the Eq Impulse is computed using both the Channel Estimation Sequence portion of the preamble and the data symbols. The latter option is typically more accurate.

The result length will be four times the FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. length so a total of 1024 points.

This is similar to, but not the same as, the Digital Demod Eq Impulse Response. The differences are:

See Also

Ch Frequency Response (802.16 OFDM)

Available Trace Data (802.16 OFDM)