Restrict bandwidth to standard values (802.16 OFDMA)
Selected (See OFDMA Standard Presets Table)
The selects between standard bandwidth configuration and manually specifying the signals bandwidth parameters.
overrides the IDCell with the PermBase value.
the bandwidth parameter setup is simplified by coupling the , , and to standard compliant values, listed in the Nominal Bandwidth droop-down list.
the bandwidth parameters, ,, and (on the tab) can be specified manually for non-standard values.
See Also