Advanced Tab (802.16 OFDMA)
The tab specifies advanced parameters to manipulate the demodulator configuration parameters (such as, adjusting the symbol timing) and the trace data results (such as, specifying unique measurement data regions or whether to include error correction in the computed data results).
The tab configures these parameters:
- Enable additional demodulator settings
- Restrict bandwidth to standard values
- Compensation
- Display Options
- Decoding (Downlink only)
- DL-MAP Decoding (Downlink only)
- UL-MAP Decoding (Downlink only)
- Decode to Map (Downlink only)
- Data Tone Modulation
- Equalizer Training
- Preamble only (Downlink only)
- Preamble, pilots and data (Downlink only)
- Preamble and pilots (Downlink only)
- No equalization (Uplink only)
- Pilots and data (Uplink only)
- Pilots only (Uplink only)
- Enable Equalizer Smoothing Filter
- Pilot Tracking
-
Subcarrier Subset Selection (Uniform Zone Analysis mode only)
- Standard Interpretation
See Also
IEEE 802.16 OFDMA Demod Properties Dialog Box