Frame Length (802.16 OFDMA)
:243.14285714286 us (See OFDMA Standard Presets Table.)
The parameter specifies the OFDMA frame length in units of time.
The property can be used to set the to a value specified in the OFDMA standard or you can specify an arbitrary value manually in the parameter.
See Also