Format Tab (802.16 OFDMA)
The tab provides access the 802.16 OFDMA signal format configuration parameters. Use these parameters to configure the VSA to match the basic signal characteristic and frame parameters of the OFDMA signal. A standard preset can be set which auto-configures the VSA to a standard specification or the setup parameters can be specified manually.
The tab dialog box configures these parameters:
- Preset to Standard
-
Subframe Type
- Standard
- Bandwidth
- Guard Interval
- Frame (Downlink only)
- Preamble (Downlink only)
- Subchannel Group Bitmask (Downlink only)
See Also