Include inactive Antenna Paths on MIMO Traces (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
includes inactive antenna paths into the STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively./MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. OFDMA analysis. This ability is helpful when the power difference between antenna paths is greater than 20 dB.
: Ch Frequency Response Trace displays overlays of all antenna paths, regardless of how low in power they are.
: Ch Frequency Response Trace displays only the results of active antenna paths.
See Also