Override Transmit Antenna Pilot Pattern (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
: 0,1,2,3
The parameter specifies whether the VSA uses auto-detection or manual mode to determine the transmitting antenna for STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively./MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. analysis measurements. The STC/MIMO measurement results can be viewed in the MIMO Info trace.
: Manually specify which antenna the VSA uses as the transmit antenna:
(default): The VSA will auto-detect which antenna is the transmitting antenna.
|
|
0 |
Antenna 0 is the measurement transmit antenna |
|
|
1 |
Antenna 1 is the measurement transmit antenna |
|
|
2 |
Antenna 2 is the measurement transmit antenna |
|
|
3 |
Antenna 3 is the measurement transmit antenna |
The STC parameter only applies to zone measurements.
Creating a manually configured STC/MIMO zone definition
The STC/MIMO zone definition are configured using the and parameters in the Zone Definition Panel.
See Also