Include Zone Offset (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
(applies to only)
tells the demodulator to assume that the zones in the Uplink Subframe prior to the current zone are not empty.
: For synchronization purposes, the demodulator assumes zones prior to current zone are not empty, and they are bypassed over.
: For synchronization purposes, the demodulator assumes zones prior to current zone are empty.
See Also