Time Tab (802.16 OFDMA)
The tab configures the signal capture parameters. These parameters are used to specify the measurement frame or to isolate a segment of the frame for further viewing and data analysis. These parameters control the pulse search or manual sync search capabilities.
The tab dialog box configures these parameters:
- Acquisition
- Acquisition Length
- Analysis Offset
- Pulse Search
- Sync Search Offset (Uplink only)
- Include Zone Offset (Uplink only)
- Override Measurement Region (demodulation)
See Also