Sync Search Offset (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
(applies to only)
manually specifies the uplink synchronization data region.
-
(manual mode): the uplink sync search data region is specified in the text box.
-
(auto mode): the uplink sync search data region is determined automatically.
The start of the data region (or window) is specified for uplink synchronization (in symbols) relative to the pulse search (when is selected) or trigger (when is cleared). The uplink sync search algorithm operates over a one-symbol search window starting at, relative to the pulse search (when is selected), or trigger location (when is cleared).
Manual mode
Using the manual mode (selected) to specify an uplink synchronization data region also depends on the setting. The Pulse Search parameter effects the operation of the manual mode as described below:
-
-selected (ON)
When is selected, the VSA assumes the signals RF Radio Frequency: A generic term for radio-based technologies, operating between the Low Frequency range (30k Hz) and the Extra High Frequency range (300 GHz). envelope is coincident with "active" bursts in the zone definition. allows skipping from the start of the RF envelope to the first active slot.
-
cleared (OFF)
When is cleared, the VSA assumes that the trigger is aligned with the start of the zone. allows skipping from trigger to the actual start of the zone.
See Also