Data Tone Modulation (802.16 OFDMA)
:16-QAM Quadrature Amplitude Modulation (See OFDMA Standard Presets Table.)
Thespecifies the data tone modulation format for the data burst.
options are:
- 16-QAM
- 64-QAM
- QPSK Quadrature phase shift keying
This parameter is NOT available when Disable Data Tone Modulation Autodetect on the tab is selected.
See Also