Enable Defined Burst Boosting Levels (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
(applies to only)
determines whether the Boosting Levels are determined automratically or manually.
: Boosting levels are automatically determined
: Boosting levels are set in the Boosting Level parameter.
See Also