Boosting Level (802.16 OFDMA)
: 0 dB (See
OFDMA Standard Presets Table.)
(applies to only)
specifies the boosting level for the data bursts. The Enable Defined Burst Boosting Levels check box
is only available for the Subframe Type in Data
Burst Analysis mode ( on the tab selected).
The data burst affects the magnitude of data subcarriers used by the data burst. The pilot tones are not affected unless using (only applies to AMC Adaptive Modulation and Coding Definition Zone types).
See Also