STC Matrix (802.16 OFDMA)
: A (See
OFDMA Standard Presets Table.)
(applies to only)
STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively. specifies the matrix type used by the analyzed zone.
The available options are:
- A
- B
- C
STC is only available for the Zone Definition.
See Also