STC Mode (802.16 OFDMA)
: No STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively./MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. (See
OFDMA Standard Presets Table.)
(applies to only)
STC specifies the STC mode used by the analyzed zone.
The available options are:
- No STC/MIMO
- 2 Transmit Antennas
- 3 Transmit Antennas
- 4 Transmit Antennas
STC is only available for the Zone Definition.
See Also