Pilot Pattern (802.16 OFDMA)
: A (See OFDMA Standard Presets Table.)
(applies to only)
specifies the STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively./MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. burst pilot pattern.
The available Pilot Pattens are:
- : Pilot pattern A used for this burst.
- : Pilot pattern B used for this burst.
is only available for Zone Definition type.
See Also