STC Mode
: None (See OFDMA Standard Presets Table.)
(applies to only)
specifies the STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively. encoding on the selected burst.
- : No STC encoding on the burst.
- : CSM (Collaborative Spatial Multiplexing) encoding on the burst.
When C-SM Spatial multiplexing: a transmission technique in which data streams are transmitted on multiple spatial channels that are provided through the use of multiple antennas at the transmitter and the receiver. encoding is active (selected), the desired Pilot Pattern can be selected for the defined burst.
is only available for Zone Definition type.
See Also