Enable Burst Analysis (802.16 OFDMA)
: Selected (See OFDMA Standard Presets Table.)
is used to set the VSA zone analysis mode between Data Burst Analysis mode and Uniform Zone Analysis mode.
: The VSA is set to Data Burst Analysis mode.
: The VSA is set to Uniform Zone Analysis mode.
is only used in Manual or Map file Definition Source mode. is not available (greyed) in Auto-detect Definition Source mode.
See Also
Manual (Definition Source) (802.16 OFDMA)