CCDF (802.16 OFDMA)
trace data is the complementary cumulative distribution function (CCDF Complementary Cumulative Distribution Function) for the selected input channel.
The is computed from the Time trace waveform. Details about how the trace data is selected aslo apply to the data used for the CCDF trace.
The is computed from the time waveform described in the trace. Details about how the trace data is selected also apply to the data used for the trace.
The VSA plots using units of percent (%) for the y-axis and power (dB) for the x-axis. Power on the x-axis is relative to the signal average power, so 0 dB is the average power of the signal. Therefore, a marker readout of
Trace A Marker 2 dB 12 %
means there is a 12% probability that the signal power will be 2 dB or more above the average power.
For more information, see CCDF trace data.
See Also