CDF (802.16 OFDMA)
trace data displays the cumulative distribution function (CDF Cumulative Distribution Function: The cumulative probability that a parameter will be less than a given value X.) for the selected input channel. CDF is computed by integrating the PDF 1) Probability Density Function Trace Data, or 2) Portable Document Format (PDF) created by Adobe Systems is an open standard for document exchange. (Probability Density Function). is explained in online help for the CCDF trace data.
The is computed from the time waveform described in the trace. Details about how the trace data is selected also apply to the data used for the trace.
See Also