Data Burst Info (802.16 OFDMA)

(Data Burst Analysis mode only)

Data Burst Info trace data shows summary data for the active Data Bursts for the Zone that is currently being analyzed. The Data Burst Info trace only reflects information for the data bursts that are analyzed.  When Manual or Map file Definition Source mode is used, the set of bursts to be analyzed is user-selectable, see the Zone Definition tab for more information about selecting data bursts for analysis. When Auto-detect Definition Source mode is used, all detected bursts are analyzed. The Data Burst Info trace provides the following results


Zone Information:


Data Burst Information:

Downlink: 

TotalPwr(dBm) = DPwr(dBm) + 10*Log(NumBurstDataSubcarriers)

Uplink:

TotalPwr(dBm) = 10*Log((NumBurstDataSubcarriers / NumBurstSubcarriers)  *
(10^(DPwr(dBm)/10)) + (NumBurstPilotSubcarriers / NumBurstSubcarriers)  *
(10^(DPwr(dBm)/10)))

Uplink(Data): 

TotalDataPwr(dBm) = DPwr(dBm) + 10*Log(NumBurstDataSubcarriers)

Uplink(Pilot): 

TotalPilotPwr(dBm) = PPwr(dBm) + 10*Log(NumBurstPilotSubcarriers)

where:

When the VSA is set to Uplink Auto-detect Zone Definition mode; the auto-detected FFB burst is analyzed as a data burst.


Uplink CDMA Burst Data Results

For Uplink analysis, defined or auto-detected CDMA Code Division Multiple Access: One of several digital wireless transmission methods in which signals are encoded using a specific pseudo-random sequence, or code, to define a communication channel. A receiver, knowing the code, can use it to decode the received signal in the presence of other signals in the channel. This is one of several "spread spectrum" techniques, which allows multiple users to share the same radio frequency spectrum by assigning each active user an unique code. CDMA offers improved spectral efficiency over analog transmission in that it allows for greater frequency reuse. Other characteristics of CDMA systems reduce dropped calls, increase battery life and offer more secure transmission. See also IS-95. regions are analyzed and the following information is provided on the Data Burst Info trace:

CDMA region analysis is only performed in UL Up Link (reverse link: from cell phone to base station)-PUSC zone types. In UL-AMC and UL-OPUSC, CDMA regions are not analyzed.

Additional signal qualty metrics

For additional EVM Error vector magnitude (EVM): A quality metric in digital communication systems. See the EVM metric in the Error Summary Table topic in each demodulator for more information on how EVM is calculated for that modulation format. and RCE metrics see the following summary tables:

Frame Summary  Table

Available Summary Data Table

See Also

Available Trace Data (802.16 OFDMA)