Burst Power is Per-subcarrier (802.16 OFDMA)
Selected (See OFDMA Standard Presets Table)
property allows you to select how the Data Burst power results in the Data Burst Info summary table are computed. The data burst power results can be computed as a per-subcarrier power level or as total power over the measurement interval.
Selected: The Data Burst power results are computed as per-subcarrier power metric.
Cleared: The Data Burst power results are computed as total power over the measurement interval.
The Data Burst Info summary table provides different data results for two power results, the DPwr(Dbm) and PPwrBm) results, depending on the setting as shown in the following table:
|
Data Burst Info Summary Table |
||
| Cleared | PTotPwr(dBm)* | |
| Selected |
DPwr(dBm) |
PPwr(dBM)* |
| * Uplink only | ||
See Also