DL-MAP Info (802.16 OFDMA)
The trace the shows the data results of the feature. Thetrace is a summary table of the downlink subframe, decoded FCH and decoded DL-MAP downlink map: A MAC message that defines burst start time for both time division multiplex and time division multiple access (TDMA) by a subscriber station (SS) on the downlink. messages. When is not selected in the current configuration, a “NO DATA” message will show, and the results will be filled with "***" asterisks.
The parameter must be selected to view the trace data results.
The trace data results include the decoded FCH parameters, a DL Down Link (forward link: from base station to cell phone)-MAP Status indicator, the decoded DL-MAP parameters, and the decoded DL-MAP_IE messages. A “NO DATA” trace message will show, and the results will be filled with “***” placeholders if DL-MAP decoding is not selected in the current configuration.
Decoded FCH parameters:
- FCHType: Normal or FFT128
- UsedSubch: A value between [0 thru 63] indicating the used subchannel bitmap.
- DLMAPType: Normal or Compressed,
- Length: DL-MAP length in slots)
- CodingType: Coding used by the DL-MAP; CC and CTC are supported, others may be indicated if specified in the FCH, but subsequent decoded DL-MAP parameters would not be valid)
- RepCode: 0=None(1x), 1=2x, 2=4x, 3=6x
Status: DL-MAP Status indicator results
- DECODED: Successfully decoded the FCH and the DL-Map messages.
- CRC Cyclic Redundancy Check_FAIL: Indicates the DLMAP CRC failed, and further DLMAP parsing was aborted.
- FCH_FAIL: Indicates the FCH was not correctly decoded, and therefore DLMAP decoding was not attempted.
- PARSE_FAIL: Indicates either the DLMAP CRC check could not be performed (DLMAP PDU (protocol data unit) The data unit exchanged between peer entities of the same protocol layer. On the downward direction, it is the data unit generated for the next lower layer. On the upward direction, it is the data unit received from the previous lower layer. bits not available to compute the CRC), or the DLMAP CRC was validated, but the decoder could not parse the entire DLMAP message. This may be due to DLMAP features of the DUT Device under Test: An acronym used to describe some type of electrical apparatus connected to test instrumentation. The apparatus can range from a single component to a complex subsystem such as a mobile phone, base station or MSC. that are not implemented in the analyzer, or due to invalid implementation of the DLMAP message by the DUT.
Decoded DL-MAP parameters:
- FrameLen: Frame length indicated in seconds.
- DLSubframe: Length of downlink subframe including preamble, in symbols.
- Frame: Frame counter
- DCDCount: DCD downlink channel descriptor: A MAC message that describes the PHY characterstics of a downlink channel. counter index to apply when using this DLMAP.
- BSID: Unique 12-hex-character value to identify the transmitting base station.
- NumIEs: (the total number of IEs counted in the decoded DLMAP)
Decoded DL-MAP_IE list:
The Decoded DL-MAP_IE list, in the lower section of the trace, includes a one-line text summary of each encountered IE (Information Element). The following IE types will be interpreted, other IE types present a textual summary of the basic IE parameters and the first few bytes of the message.
- Nornal BURST IE
- STC Space Time Coding (STC) allows the transmitter to transmit signals (information) both in time and space, meaning the information is transmitted by two antennas at two different times consecutively. Zone Switch IE
- CID connection identifier: A 16-bit value that identifies a transport connection or a uplink (UL)/downlink (DL) pair of associated management connections (i.e., belonging to the same subscriber station (SS) to equivalent peers in the MAC of the base station (BS) and subscriber station (SS). The connection identifier (CID) address space is common (i.e., shared) between UL and DL. Security associations (SAs) also exist between keying material and CIDs. See also: connection_Switch IE
- MIMO Multiple Input, Multiple Output: A physical layer (PHY) configuration in which both transmitter and receiver use multiple antennas. Basic IE
See Also