DL-MAP Decoding (802.16 OFDMA)
: Cleared (See OFDMA Standard Presets Table.)
(applies to only)
will decode the DL-MAP downlink map: A MAC message that defines burst start time for both time division multiplex and time division multiple access (TDMA) by a subscriber station (SS) on the downlink. messages of the downlink subframe and report the interpreted results in the DL-MAP Info trace. DL Down Link (forward link: from base station to cell phone)-MAP decoding will accommodate Normal or Compressed mode DL-MAP messages encoded with either CC (convolutional coding) or CTC (convolutional turbo coding) encoders.
The function will operate differently depending on the OFDMA zone definition mode: or Definition Source mode:
-
:
Auto-detect Definition Source mode uses the feature to decode and interpret the FCH and DL-MAP to dynamically provide a downlink subframe zone definition for analysis for each measurement. When is selected, DL-MAP Decoding is always performed so the checkbox is not available (greyed). Use the DL-MAP Info trace to view the decoded FCH and DL-MAP data results.
-
and :
When the VSA is set to (or DefinitionSource mode, the feature operates independent of the current measurement analysis configuration. This allows the measured DL-MAP map message information to be viewed independent of the Definition Source parameter settings. The zone and zone must include the complete FCH and DL-MAP regions within the analyzed subframe for the feature to perform correctly.
: Automatic DL-MAP decoding is performed.
: Automatic DL-MAP decoding is not performed and the property is disabled (greyed).
The VSA also provides UL-MAP Decoding.
See Also