Inst Spectrum (802.16 OFDMA)
shows the frequency spectrum of the trace. This data is the instantaneous (pre-demodulated) spectrum of the input signal, the same as Digital Demod Inst Spectrum. If averaging is not on, this is identical to the data (refer to the Digital Demodulation Block Diagram.
See Also