IQ Ref (802.16 OFDMA)
(IQ Reference) shows reference data with one point per subcarrier per analyzed IEEE Institute of Electrical and Electronics Engineers. A US-based membership organisation that includes engineers, scientists, and students in electronics and related fields. The IEEE developed the 802 series wired and wireless LAN standards. Visit the IEEE at http://www.ieee.org 802.16 OFDMA symbol time.
uses a multi-color display to distinguish the data results, for more information about the trace data symbol colors, see the About Trace Data topic.
See Also