ACP Overall (Adjacent Channel Power)
The table lists the available summary data for the ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. measurement. When measurement averaging is enabled, the values in ACP Overall are computed from the averaged detected spectrum data, and the averaging type and count (e.g.," RMS:10") are displayed at the top of the trace's display. See ACP Spectrum Trace Data Block Diagram and Detectors and Power Spectrum Analysis for more information.
Total Carrier Power - The total measured power of all enabled carriers (see ACP Carrier Info)
Total Integration Bandwidth - The sum of integration bandwidth used for measuring the Total Carrier Power metric.
Total Carrier PSD Power Spectral Density: See power spectral density. - The total measured power spectral density of all enabled carriers (see ACP Carrier Info)
Limit Test Result - The aggregate Pass/Fail status of power limit masks for all enabled offsets (see ACP Power and ACP Spectrum)
Querying summary table data results programmatically
To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.
See the How To Query Summary Table Data Results topic for more information.