ACP Carrier Info (Adjacent Channel Power)
The table shows power measurement information about Carriers configured for the Adjacent Channel Power measurement. When measurement averaging is enabled, the values in ACP Adjacent Channel Power: The power from a modulated communications channel that leaks into an adjacent channel. This leakage is usually specified as a ratio to the power in the main channel, but is sometimes an absolute power. Carrier Info are computed from the averaged detected spectrum data. See ACP Spectrum Trace Data Block Diagram and Detectors and Power Spectrum Analysis for more information.
ACP Carrier Info is a type of Matrix Table that provides sortable rows by column, selectable column visibility, and copy/paste and export functionality to share rows of content or complete tables to applications like email, text editing or spreadsheet programs.
| CC | Carrier Power (dBm deciBels referenced to a milliWatt: dB relative to 1 milliwatt dissipated in the nominal input impedance of the analyzer) | Integ BW (Hz) | Carrier PSD Power Spectral Density: See power spectral density. (dBm/Hz) | Filter | Offset Freq (Hz) | Measure | Bandwidth (Hz) |
|---|---|---|---|---|---|---|---|
|
identifies the carrier for the row (corresponds to the Carrier parameter tab). |
is the average power of the carrier. See Carrier parameters for details about configuring the carrier power measurement. |
Integ BW is the bandwidth used for the average power measurements, as defined by Carrier parameters. |
is the average power spectral density of the carrier. See Carrier parameters for details about configuring the carrier power measurement. |
indicates what filter factor is applied to the carrier power measurement. |
is the frequency location of the center of the carrier relative to the Carrier Reference Frequency. |
indicates if the carrier power is measured (‘ON’) or not (‘OFF’). |
indicates the expected carrier bandwidth (corresponds to the Span property of the carrier definition). |
See Also