Interfering Signals Tab (Spectral Emissions Mask)
Interfering Signals Tab
Allowable Interfering Signals
Index - Indicates the automatically assigned interfering signal number, starting with 0. When an interfering signal's checkbox is selected, it is included in the measurement.
Span - Sets the span of the interfering signal. Units are Hz.
Default: 0 Hz
Offset from Edge - Sets the offset frequency from the edge of sub block. Units are Hz.
Default: 0 Hz
Offset Side - Sets which side of interfering signal is present.
Lower - Frequency region is below the reference carrier.
Upper - Frequency region is above the reference carrier.
Default: Upper
Choices: Lower, Upper
Subblocks - Sets the ID(s) of the subblock(s) the selected interfering signal is referencing (Subblock1, or both Subblock 1 and Subblock2).
Default: 0 (Subblock1)
Inner Offset - Sets a value indicating whether this interfering signal is at an inner offset area or not.
Default: False
- Deletes the selected interfering signal.
- Adds an interfering signal to the end of the collection.
- Deletes the entire collection of interfering signals.
See Also
Spectral Emissions Mask Properties Dialog Box