SEM Summary (Spectral Emissions Mask)
The table lists the available summary data for the SEM measurement. When measurement averaging is enabled, the values in SEM Summary are computed from the averaged detected spectrum data, and the averaging type and count (e.g.," RMS:10") are displayed at the top of the trace's display. See the SEM Spectrum Trace Data Block Diagram and Detectors and Power Spectrum Analysis for more information.
Total Carrier Power - The total measured power of all enabled carriers (see SEM Carrier Info)
Total Carrier PSD Power Spectral Density: See power spectral density. - The total measured power spectral density of all enabled carriers (see SEM Carrier Info)
Limit Test Result - The aggregate Pass/Fail status of power limit masks for all enabled offsets (see SEM Results and SEM Spectrum)
Querying summary table data results programmatically
To programmatically query the Trace Summary Table data results using the Summary() and SummaryUnit() methods in the MeasurementData object.
See the How To Query Summary Table Data Results topic for more information.
See Also