Analysis Tab (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Analysis

The Analysis tab provides various analysis tools and options, including selectable pulse modulation types and statistics.

Synchronization Domain -- This parameter is provided on every tab because it is a fundamental configuration parameter affecting the entire Advanced-Radar/Hopping measurement.

____________________________________________

Analysis parameters are grouped into the following panels: