Statistics Panel (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Analysis Tab > Statistics Panel

The Analysis tab's Statistics panel allows you to control all Trend, Histogram, and Cumulative Pulse Table data gathering and statistical/trace results.

Trend, Histogram, and Result Table traces that display statistical data are only available when the Synchronization Domain is Amplitude or the Pulsed checkbox is checked.  If both of these are not true, these traces won't be available for selection.

The Statistics panel allows you to set the following parameters:

See Also

Analysis tab

Pulse Table