Doppler Tab (Advanced-Radar/Hopping)

Menu Path: Analysis > Advanced-Radar/Hopping Measurement Properties > Calculation

Range Doppler enables you to use received pulses to create a Range Doppler (Velocity) Map and identify targets present in the Doppler Map. Pulses/responses must be transmitted periodically, and you must know the period at which the pulses are transmitted. You can use either Non-Segmented Capture mode or Fixed Length Segmented Capture mode.

 

Range Doppler Enabled -- Enables and disables Range Doppler Analysis.

Pulse Definition

The first step to Range Doppler is doing a matched filter on the received pulses. This matched filter convolves the input signal with the transmitted pulse which must be specified by the user.

Doppler Map

The Doppler Map properties section specifies the parameters relating to the creation of the Range Doppler Map.

Constant False Alarm Rate (CFAR)

Constant False Alarm Rate (CFAR) is a method used to find targets in a Range Doppler Map. In CFAR,each sample is tested individually (called the Cell Under Test) and compared to surrounding samples (called Training Cells). If the power of the Cell Under Test is greater than the Threshold, that cell is identified as part of a target. The Threshold is calculated by:

The Noise Estimate (Pn) is calculated by averaging the power in all of the training cells, where N is the number of training cells:

The alpha value is calculated by using the False Alarm Probability and the number of samples in the training band N:

See Also

Advanced-Radar/Hopping Measurement Properties Dialog Box