Advanced-Radar/Hopping Measurement Properties Dialog Box
Menu Path:
The dialog box lets you configure parameters for Advanced-Radar/Hopping measurements.
This dialog box is only available when the Measurement Type is set to Pulse ()
The dialog box contains tab headings that group similar configuration parameters as follows:
-
Capture Tab: Contains parameters to optimize pulse detection.
-
Detection Tab: Contains parameters that specify what part of the signal to analyze.
-
Analysis Tab: Contains parameters that specify what part of the signal to analyze.
-
Calculation Tab: Contains parameters that set the criteria for analyzing the detected pulses.
-
Doppler Tab: Contains parameters that set the criteria to use received pulses to create a Range Doppler (Velocity) Map and identify targets present in the Doppler Map.
See Also