Range Doppler Map (Advanced-Radar/Hopping)
is a doppler map created from the CIR vs Time trace by doing an FFT Fast Fourier Transform: A mathematical operation performed on a time-domain signal to yield the individual spectral components that constitute the signal. See Spectrum. vertically over each point in the CIRs. The units for this trace are determined by the Axes Units parameter. The start distance (first value on the X-axis) and center speed (center value on the Y-axis) will always be zero.
See Also