Output Power Marker Stop (Bluetooth)

Default: 80%

Output Power Marker Stop sets the end of the region used to compute the Avg Power result, expressed as a percentage of the detected burst's payload. The payload spans the decoded PDU (protocol data unit) The data unit exchanged between peer entities of the same protocol layer. On the downward direction, it is the data unit generated for the next lower layer. On the upward direction, it is the data unit received from the previous lower layer. payload only — the preamble, access address, PDU header and CRC Cyclic Redundancy Check lie outside it.

The default 20% to 80% window measures the central portion of the payload, away from the burst's power ramps and the settling that follows them.

Peak Power is not restricted to this window. It is the maximum over the whole detected packet.

See Also

Output Power Marker Start

Avg Power

Peak Power

Demod Tab