Avg Power (Bluetooth)

Avg Power is the mean output power of the analyzed burst, computed over the region of the burst's payload set by the Output Power Marker Start and Output Power Marker Stop parameters (by default the central 20% to 80% of the payload, away from the power ramps).

The standard reference for the LE output power test is Bluetooth Core Specification Vol 6, Part A, §3.1.2. Conformance testing averages the result over at least 10 packets; with averaging ON, the Average column of the Results Table provides this multi-packet mean.

See Also

Results Table

Limits Table