Burst (Bluetooth)
1
Burst selects which of the bursts detected within the Search Length is demodulated and analyzed. Burst 1 is the first burst found in the acquisition. A value higher than the number of bursts actually detected is clamped to the last detected burst, so the selection always refers to a real burst.
All detected bursts are listed in the Burst Table trace; the results in the Results Table and the demod traces are computed from the selected burst only.
See Also