Search Length (Bluetooth)

Default: 2.7 ms

Search Length sets the length of the acquired time record that is searched for Bluetooth bursts. Set the search length long enough to contain at least one complete burst of the packet type being transmitted.

The default of 2.7 ms is a 0.5 ms search window plus the 2.12 ms worst-case LE 1M packet. Increasing the search length lets the measurement find multiple bursts, which are then listed in the Burst Table and selectable with the Burst parameter.

See Also

Time Tab

Burst Search Mode