Bluetooth Demod Properties Dialog Box
The dialog box contains the parameters that configure demodulation and analysis of a Bluetooth LE burst.
The Bluetooth Demod measurement type must be selected before this dialog box is available. To enable the demodulator, click .
The section at the top of the dialog box holds the settings that are shared by both Bluetooth measurements (PHY Physical Layer family and rate, packet type, and channel index). See Common Properties for details.
The dialog box contains these tabs:
-
Demod Tab — payload pattern, PDU (protocol data unit) The data unit exchanged between peer entities of the same protocol layer. On the downward direction, it is the data unit generated for the next lower layer. On the upward direction, it is the data unit received from the previous lower layer. whitening, and output power marker settings.
-
Time Tab — burst search mode, search length, and burst selection.
See Also