Correction (Bluetooth Spectrum)
is the correction curve derived from the calibration data. It is applied to the acquired data to compensate for the frequency response of the input hardware and the input digital filtering, correcting phase and magnitude anomalies in the analyzer’s hardware and software signal processing.
This trace is available only while the measurement’s active input domain is . See Preferred Input Domains.
See Also