Raw Main Time (Bluetooth Spectrum)

Raw Main Time is the raw data read from the input hardware or playback file, before time corrections and software resampling:

Raw Main Time data is useful when hardware trigger types are used (to see what caused the trigger) and when a recording is played back (to see exactly the samples saved in the recording).

See Also

Available Trace Data