Inst Eq Ch Frequency Response (Channel Sounding)
shows the channel response for the Symbol Rate bandwidth of the signal for each measurement update, regardless of averaging. The averaged version of the equalized channel frequency response is shown in the Eq Ch Frequency Response trace. This trace can be copied to a data register and used with the User Corrections > Fixed Equalization feature to compensate for the measured channel.
See Also