Troubleshooting Component Test Measurement

This topic contains information to help you troubleshoot component test measurement. You should also review Making a Component Test Measurement for additional measurement information.

 

PROBLEM

POSSIBLE CAUSE

SOLUTION

Measurement fails to lock on signal

Signal not present.

Check connections

 

Carrier too far from center frequency.

Adjust center frequency.

 

Signal has inverted frequency spectrum

Check the Mirror Frequency Spectrum setting (Analysis > Frequency tab).

See Also

Making a Component Test Measurement

Error and Status Messages

About Troubleshooting