Stim AM/PM (Component Test)
The trace is the source-side counterpart to AM/PM: the stimulus source channel's response-minus-stimulus phase (degrees) versus stimulus magnitude (Vpk), with a least-squares polynomial fit of order Polynomial Order. The fit coefficients are reported in the Linearity Summary table.
This trace only has contents when Reference = Measured Stimulus and Computation Mode = Statistical, and requires phase compensation to be enabled; otherwise it shows no data.
See Also