Stim Eq Error Vector Time (Component Test)

The Stim Eq Error Vector Time trace is the equalized, source-side counterpart to Error Vector Time: the normalized error vector, in percent, between Stim Eq IQ Meas and Stim Eq IQ Ref after the estimated linear channel response is compensated.

This trace only has contents when Reference = Measured Stimulus and Computation Mode = Statistical.

See Also

Eq Error Vector Time

Stim Error Vector Time

Available Trace Data