Format Tab (Custom IQ)
The Format tab of the Custom IQ Demod Properties dialog box lets you configure the demodulator for Custom IQ signals. These are the parameters necessary for the VSA to lock on to and demodulate the test signal.
The Format tab dialog box enables you configure these parameters:
Quick Setups
Format Parameters
- Constellation
- Edit (Constellation Editor)
- Recall (Constellation File)
- Save (Constellation File)
- Symbol Rate
- Result Length
- Search Length
- Pulse Search Enable
- Pattern Search Enable
- Enable Cross-Correlated EVM
See Also