Making a Custom IQ Measurement

This topic describes how to configure the VSA to make a Custom IQ measurement.

Overview

You must manually configure the VSA Custom IQ demodulator to measure your signal. To do so, configure the measurement setup parameters, e.g. constellation, symbol rate, result length, etc.

Signal Setup

Before selecting the Custom IQ demodulation mode, make sure that the input signal is correctly captured by the analyzer. Specify the VSA basic signal measurement setup parameters so that the input signal is fully captured including; the center frequency, span, input range, etc.. You can use the Spectrum and Time traces to verify that the signal of interest is properly captured.

Demo Signals

To use a demo signal, click File > Recall Demo > navigate to the "%PROGRAMFILES%\Keysight\89600 Software <ReleaseVersion>\89600 VSA Software\Help\Signals\CustomIQ" folder and select a Demo File.

Configuring the Demodulator

Step 1 - Specify the signal parameters

To begin, select the Custom IQ demodulator, click Analysis > Type > General Purpose > Custom IQ. Then open the Custom IQ Demod Properties dialog, click Analysis > Custom IQ Demod Properties.. .

Loading a demo signal file like"v29-8qam.htm" will auto-select the Custom IQ demodulator.

Step 2 – Configure the Measurement Parameters

The setup options for the Custom IQ demodulator are similar to other demodulation formats; however, the Custom IQ demodulator provides the ability to create an IQ constellation, set parameters, and save as a Quick Setup, or choose an existing Quick Setup and customize it to match your signal.

Format Tab

Filter Tab:

Advanced Tab:

See Also

Selecting the Custom IQ Demodulator

Troubleshooting Custom IQ Measurements